3/3/2008 8:41 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi! there is no need o initialize after SMS sending/receiving. Only once from power-off/on or restart of the cpu/modem. And if this is finished with "done". Everything is ok and you can invoke SMS sending/receiving as often as you want. If this is finished with "aborted" you have to try it up to 3 times i would say. As far as i know it IS reliable (the code), but notice: The CSD service is in principal ok, but there are many restrictions/problems caused by different modems or different providers in different countries. E.g. some states in the USA switched off the CSD service at all. You have do ensure that on your SIM card the CSD service is enabled. You have to ensure that from your Micro/WIN Station the full number is transfered to your remote station. A lot of tricky things. Did you already heard of the MD740-1 solution? http://support.automation.siemens.com/WW/view/en/24960449 Therefore you can use Teleservice via TCP/IP which is in my opinion more reliable. In case that this is to expensive for only one Remote Station or something like this you have to use the CSD Teleservice option. regards Lif |
3/5/2008 12:42 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi, where is there a staement with the content of "invoking initialization subroutine every xx seconds/minutes. You can use it with S7-200! but you need there an additional Ethernet CP. Mall regards Lifrasil |