7/2/2015 12:36 PM | |
Posts: 2 Rating:
|
Hi! How to configure two connections - master&slave in S7-400H with CP443 (CP 443-1 Advanced - 1GX20 V2.1) 1 - Master M104 - data collection (S7IEC_M104_CP443 V1.3c Rel_110610) 2 - Slave S104 - transmit data to HMI (S7IEC_S104_CP443 V1.3c Rel_110610) CFC error that block types FB100 have different properties and asks to replace a block in the library CFC. In this case, the master block rewritten slave block and master block not work. they work separately how to run them simultaneously in a controller on a same IP address, but different ports ? ---------------------------------------------------------------------------------------------------- Split from IEC104 for S7-400H. |
Last edited by: elochkin at: 7/2/2015 12:37:11 PMLast edited by: Min_Moderator at: 7/2/2015 2:24:05 PMNew subject after splitting |
|
4/14/2017 10:59 AM | |
Joined: 1/23/2013 Last visit: 10/17/2024 Posts: 38 Rating:
|
You need to do rewire in library, then is possible import to project |
Follow us on