9/22/2012 1:22 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Ahmed; You cannot talk to multiple slaves simultaneously, but you can talk to them one after the other. Remember that you need to set the Modbus Function parameters (different for each type of Modbus Function) in the Send Source DB. This is all well explained in the Modbus RTUmaster manual: SIMATIC S7-300/S7-400 Loadable Driver for Point-to-Point CPs: MODBUS protocol, RTU format, S7 is master |
11/8/2012 12:20 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Ahmed; There are many, many threads on the subject in the forum. In this particular one you will find a project designed by member DR75 that might help you understand the mechanics of multiple slave polling with a Siemens Modbus RTUmaster: Multiple Modbus RTU slaves with CP341/CP441? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/8/2012 12:22 PM |
|
Follow us on