12/13/2021 4:20 PM | |
Joined: 10/7/2021 Last visit: 1/16/2023 Posts: 6 Rating: (0) |
Good Afternoon, What is the maximum amount of analog input cards i can attach to the Simens LOGO 8.3? Alex |
12/13/2021 4:43 PM | |
Joined: 10/7/2021 Last visit: 1/16/2023 Posts: 6 Rating: (0) |
ok cool thanks, So if i use the x4 on the base model i can then only add x2 2ai expansions. Alex |
Follow us on