11/16/2012 11:31 AM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello, All answers are in the Logo Manual Chapter 2. Regards, Marcjan |
Problem solved? |
|
11/16/2012 11:44 AM | |
Joined: 8/18/2009 Last visit: 11/25/2024 Posts: 549 Rating: (33) |
ThanksMarcjan, I have seen in manual that maximum 2 AO (only one AO Expansion Module) we can use in logo. I have 4 AO so logo is not compatible ... Please tell me & clear my doubt.. Also I wantlogging display in XL fomat in their PC for 4 AI & 4 AO value only( Max.8 data) so using this Logo PLC which is economical OPC client required tologging display in XL fomat in PC. |
Last edited by: RAJKIRAN at: 11/16/2012 11:55 AMLast edited by: RAJKIRAN at: 11/16/2012 11:48 AMLast edited by: RAJKIRAN at: 11/16/2012 11:46 AMRajkiran Patil |
|
4/18/2017 8:03 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by edwin saputra is split to a separate thread with the subject Maximum expansion module connect to LOGO! 8 Best regards |
Follow us on