2/19/2013 11:16 AM | |||||||||||||||||||||||||||||||||||||||||
Joined: 2/6/2009 Last visit: 1/7/2025 Posts: 939 Rating:
|
Hi, Here is the list of communications possible with CPU 315-2PN/DP. As per the below list you can connect 15 numbers of HMI's.
Check the complete specification of any CPU for its details. Here is thelinkfor CPU 315 2PN/DP.
|
||||||||||||||||||||||||||||||||||||||||
Last edited by: Saravana kumar at: 2/19/2013 11:18 AM_______________________________________________________________ |
|||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to
1 thankful Users |
2/19/2013 11:51 AM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
What does it mean "Adjustable" -http://support.automation.siemens.com/WW/view/en/23369901 Just in case! Best regards, Hristo Mihalev
|
2/19/2013 12:56 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi If more then 15 connections are required then use CP. More detailshere! Also sum of PG,OP and S7 connections shall not be larger then maximum number of connections. So if PG communication is set to 1 and S7 connections 2 then max OP connectios would be 13 in case of 315-2DP |
Last edited by: manmeet at: 2/19/2013 1:19 PMLast edited by: manmeet at: 2/19/2013 1:19 PM |
|
Follow us on