4/10/2016 11:16 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
yes this is the data. the PLC can control max 16 nums of et200 stations. |
This contribution was helpful to1 thankful Users |
4/10/2016 11:17 AM | |
Joined: 12/15/2015 Last visit: 5/31/2016 Posts: 147 Rating: (3) |
Thank you !
|
4/10/2016 7:33 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306)
|
Can you please provide more information regarding, what is the basis if this conclusion ? |
Last edited by: Navnag at: 4/10/2016 7:34:02 PMLast edited by: Navnag at: 4/11/2016 4:57:07 AMThere is no such thing as the last bug in a program |
|
4/10/2016 8:30 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
Hello, @Navnag 2.) each ET200 IM (Interfacemodule) presents 1 Slave or 1 IO-Device, so if the PLC Data I can't understand why such a question is asked! Regards |
4/10/2016 9:05 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Is it a real or hypothetical question? For these type of question you can simply see data sheets. To write an ideal answer, you need someone to get all data sheets for all CPUs S7-300, 1200 & 1500 and tell you how many station each CPU can be linked with! If you are still in design phase of your project and need a help, you can tell us how many stations you will connect your CPU to and if it's PRofibus or Profinet or mix and then we can tell you the suitable CPU. |
Ayman Elotaify |
|
Follow us on