9/14/2016 3:15 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Maene; Would it help if you were told that connections for PUT/GET communication functions were listed as "S7 communications"? Basically, you cn reserve up to 14 connections for all your S7 Communications (including one-sided connections for PUT/GET); the rest of the 32 connections available for your CPU are distributed between PG connctions (1 reserved by default), OP connections (1 reserved by default) and S7 Basic Communication connections. See here for more information: CPU-CPU communications with Simatic controllers: https://support.industry.siemens.com/cs/om/en/view/78028908 How are the communication resources assigned in the S7-300? https://support.industry.siemens.com/cs/om/en/view/97649464 Hope this helps, Daniel Chartier |
Follow us on