12/10/2015 8:21 AM | |
Joined: 6/14/2014 Last visit: 8/8/2022 Posts: 27 Rating:
|
Hi Guys, For me the same challenge. I've to log the data from ±10 tags. The time span will not be 90 days like Om@ir, but must be longer than a weekend. So the customer can monitor the process on a monday from the weekend. The setup will be the same. A 1215 CPU with a KTP700 2nd generation basic panel. Now I still have some questions about the 10000 entries from the basic panel. Is this a limitation that excists by the firmware off the panel, or is it a memory issue that can be solved with a USB-stick inserted in the panel? The second and last question: The 10000 entries is the total per each tag, or for all the tags that will be logged? Kind Regards, RickL |
Follow us on