9/21/2016 8:05 AM | |
Posts: 67 Rating:
|
Hello All, I have to connect S7-1200 with ModScan via (Modbus TCP/IP) the ModScan is the Server , then i wil to be the client In my example i try to connect via modscan program ... but unfortunately i got msg connection failed, i followed several examples in the forum, but still the problem not solved, could anyone please check the attached photos and help me where i do something wrong ? PLC s7-1200 1214 AC/DC/RLY V4 MB_Client V4 AttachmentTCP_SCREENSHOT.zip (74 Downloads) |
Follow us on