11/28/2014 12:07 PM | |
Posts: 21 Rating:
|
Hello Program is the same as example in online help of MB_CLIENT i think it doesn't work like this because of the change on the request input. Regards EDIT: as i see in new examples explains that you have to use one MB_Server for each connection, with diferent ID, and IP_port, i don't understand why because only one MB_Server should allow multiple connections as other devices right? |
Last edited by: cgarciaaguam at: 11/28/2014 5:06 PM |
|
12/11/2014 1:44 PM | |
Posts: 21 Rating:
|
Find attached pictures of the program (server and client) I see more people with the same fault 80A3, also as i said now mb_client function doesn't work like flanges in the request input like previous versions. Regards AttachmentModbus TCP V13.zip (372 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on