4/18/2017 2:24 PM | |
Posts: 24 Rating: (1) |
Dear Team, I am facing a similar problem. I am using software PCS 7 V8.0 SP2. I am trying to establish Modbus TCPIP communication with Redundant 410-5H controllers as a Client. I downloaded the software library from the link https://www.industry.siemens.com/services/global/en/IT4Industry/products/simatic_add_ons/s7_open_modbus_tcp/Pages/default_tab.aspx?tabcardname=Downloads. I downloaded the setup and installed it. In my project when I try to insert the FB915 MB_PNHCL, it gives an error Parameter type S7_Array is not supported. I deleted all blocks in my project and also cleared all CFCs still I am getting the same error. Any help is appreciated. Thank You. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/18/2017 4:03:52 PMNew subject after splitting |
|
4/18/2017 3:01 PM | |
Posts: 24 Rating: (1) |
I have not renamed/rewired some of the FBs which are used for ModbusTCP communication. Any other possible solution u can suggest? |
Follow us on