6/14/2017 8:52 AM | |
Posts: 5 Rating:
|
Can anyone help me with a problem facing at my site location? I have a program which access IRC module along with CPU Ethernet port to generate Redundant communication setup for 2 different IP. We have configured MB_SERVER_DB instances in Rung 16 and Rung 19 IP A: 192.168.1.23 (CPU) IP B: 192.168.2.23 (IRC Module) However, below happens.
Can anyone help me in resolving this issue. i am currently stuck at site. AttachmentIZ MTBE AH220.zip (101 Downloads) |
6/14/2017 9:55 AM | |
Posts: 5 Rating:
|
I have used MB_SERVER_DB as DB1 for both rung 16 and 19. But since these two are in different IP ports hence i could use Port 502 for both the TCON's |
Follow us on