9/18/2019 8:12 AM | |
Joined: 10/11/2006 Last visit: 2/8/2023 Posts: 5418 Rating:
|
Hello, C = B + A because Move Relative aborts the previos command. More info: 10.6.2 MC_MoveRelative: Function chart V4 https://support.industry.siemens.com/cs/ww/en/view/109749262 |
With best regards, |
|
9/18/2019 5:55 PM | |
Joined: 5/6/2010 Last visit: 1/29/2023 Posts: 89 Rating:
|
But the units for A are opposite of B and C. One is positive and the other is negative. What I am ultimately getting at is does the system consider that the decel towards 0 speed (A) count as positive movement and have to be compensated for in B by extending the time it runs at full velocity (per the graph)? I should have stated that the picture with the graph has velocity as the Y axis and is a value of 0 at the x-axis crossing (positive above, negative below)
|
Last edited by: daynada at: 09/18/2019 17:58:59 |
|
Follow us on