7/12/2019 10:42 AM | |
Posts: 37 Rating:
|
Usecase Single axis example is a simple project that demonstrates possibility of cupping between NX MCD, SIMIT SP DEMO and PLCSIM Adv. It includes MCD model of TO PositioningAxis, TIA portal project with configured SINAMICS V90 drive and SIMIT project with Telegram3 chart created in SIMIT SP DEMO environment. Features
Implementation The single axis model consists of motor with encoder, rotary-gear, worm-gear and carriage slider that moving along the linear axis. Rigid bodies for the master and slave gears as well as for the cart are defined in NX MCD model. Each rotary-gear is assigned to the Hinge Joint and the slider is connected to Linear Joint. Upper and lower limits of the Linear Joint are set to 370 mm and 0 mm correspondingly. Rotary-gear ratio is 12:6 and lead-screw pitch is 10 mm/rot. Speed Control attached to the master gear simulate the motor with encoder. Carriage slider position could be obtained from Sliding Joint. Usage
AttachmentSingleAxis.zip (1370 Downloads) |
Last edited by: digiSUPport at: 07/15/2019 13:09:24 |
|
This contribution was helpful to
3 thankful Users |
7/15/2019 1:26 PM | |
Posts: 37 Rating:
|