7/7/2016 9:00 PM | |
Posts: 19 Rating: (0) |
Dear all, I'm having a similar problem: every cca 3 minutes my MD 720-3 does the restart routine (LEDs are flashing fast in a sequence). During this routine, the communication doesn't work either to the PLC or PC with terminal program. After finishing the routine, the MD 720-3 starts to work normally for next cca 3 minutes and then restarts again. This is happening all the time. I tried with loading factory settings, but this behaviour hasn't changed. The device is powered by SITOP 5A unit. Does anybody has a solution or advice? Many thanks in advance. Regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/8/2016 12:00:03 PMNew subject after splitting |
|