Industry Online Support
Technical Forum
9/26/2008 9:34 PM | |
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating: (11) |
Hi The "Reserved bits for fine resolution" parameter specifies the desired pulse multiplication of the encoder increments transmitted in actual encoder values.You can set the fine Resolution between 0- 15. Minimum fine resolution for TTL encoders A minimum fine resolution of 22 (= 4) must always be taken into account and set for TTLencoders. You need to calculate this based on encoder Parameters. The Formula is given in the manual.
|
9/26/2008 10:18 PM | |
Posts: 99 Rating: (3) |
I can read the manual but understanding the philosophy behind it... So I will take it only as a multiplier in order of 2 |
Follow us on