8/30/2022 11:12 AM | |
Joined: 3/11/2019 Last visit: 7/26/2024 Posts: 1528 Rating:
|
Dear LukPot,
You have to check the LED state of S7-1200, the LED show if program is transfered corrrectly (link down below). The CPU type must be the same. SIMATIC S7 S7-1200 Programmable controller"The RUN/STOP LED alternately flashes green and yellow to indicate that the program is being copied. When the RUN/STOP LED turns on (solid yellow) and the MAINT LED flashes (yellow), the copy process has finished. You can then remove the memory card." regards sancruz |
Feedback appreciated, please rate |
|
Follow us on