11/1/2016 6:30 PM | |
Joined: 1/23/2013 Last visit: 10/6/2024 Posts: 38 Rating: (1) |
Hi! I have 6ES7315-2EH14-0AB0 and it says in properties of CPU: 384 KB work memory; My program has totaly size in working memory 212962byte. Module information of CPU says that I still have 180kb free working memory but I can't add aditional logic because i receive error: E: 0xFFDF_0117: [S7DOS] The block/op. sys. update is too large. Exist some limitation how much working memory is dedicated to code and how much to code? BR Janez ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/2/2016 2:31:03 PMNew subject after splitting |
|
11/2/2016 7:53 PM | |
Joined: 1/23/2013 Last visit: 10/6/2024 Posts: 38 Rating: (1) |
Can be that additional code gets over limit of max. number of DB(sum DB, FC, FB) as described in CPU specification? |
Follow us on