3/16/2022 2:31 PM | |
Joined: 2/8/2022 Last visit: 4/27/2022 Posts: 5 Rating:
|
Hello everyone, I have a problem related to the memory of data logging. The problem is really just that the trend doesn't show all the values we expect. For example, we set up a data log with 50,000 data records with a logging cycle of 5 s. We should then be able to look back 2.8 days in our trend view. If we look effectively, we see that we can only see data up to 2 days ago. So, some data is lost. The ultimate goal would be to be able to collect data every second in a data log (trend view) and this for a whole week. So I want to look back a week in my trend view without any problems. Is this possible? Does anyone have other solutions?
AttachmentNieuwe map.zip (112 Downloads) |
3/24/2022 11:43 AM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15350 Rating:
|
Hello ODK The system limits for a TP1200 Comfort is 20.000 entries per log. https://support.industry.siemens.com/cs/ww/en/view/109798671/91274388747 So perhaps the system behaves like this because of to much entries for the expected log. And check also if there is only that one tag in that log, because the entries per log depends on all tags in that log Bye Murof |
Last edited by: Murof at: 03/24/2022 11:45:46If this Information really helps, you could use the Rate function |
|
Follow us on