Industry Online Support
Technical Forum
4/9/2012 7:41 AM | |
Posts: 2 Rating: (0) |
Dear sir i can use micromaster 430(37 kw)at crane hoisting systerm . insted of ativar 71 |
4/9/2012 10:34 AM | |
Posts: 29 Rating: (0) |
Please clarify your question. If you mean is it possible to use MM430 with 37 kW, instead of Ativar 71. Yes you can use if their powers match. |
4/9/2012 12:34 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
Yes you can use MM430 for your application You need to perform Quick comissioning, then set control Parameters for Start- Stop and You will get what you want Please refer Operating instruction and Parameter List for More help Please use Vector control as Control Mode because for Hoist application, encoder feedback will give you best result. For that you need Encoder Module for your drive Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on