1/24/2014 12:25 PM | |
Joined: 9/19/2009 Last visit: 3/10/2024 Posts: 458 Rating: (81) |
Hi I would like to know if is possible to use HMIRuntime.Trace in Microsoft Scritp Debugger? I´m testing script from Online -> Simulation -> Enable Script Debugger, but I can´t see my value from HMIRuntime.Trace. I´m testing with Simulation, but the target is a Confort Panel KP With WinCC is possible to see it inside GSD Diagnose Thank You |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
1/24/2014 12:48 PM | |
Posts: 1299 Rating: (135)
|
Hello, in manual they say Hmiruntime.trace is supportedforpc based applications. So I suggest it's not possible to show it on a comfort panel. I'm not sure about Microsoft Script Debugger. But as an alternative you can use "showsystemalarm". this will also work on your panel. K!ke |
1/24/2014 1:01 PM | |
Joined: 9/19/2009 Last visit: 3/10/2024 Posts: 458 Rating: (81) |
Thanks so much for your tip Ionlywant to check the Script, I don´twant show it in the Panel. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on