9/28/2015 11:07 AM | |
Joined: 9/29/2011 Last visit: 6/6/2024 Posts: 23 Rating:
|
Hi. You are talking about TIA V13 without SP1, we are using TIA V13 SP1 in order to use the simulator for the S7-1200. So it's a different thing. Most of all, you have a dual boot with windows 7 64 bits and windows 7 32 bits. As I said before, I don´t have problems running in a VM but the thing is I'm teaching students, it's no my computer, a lot of people use the computer. I want the software running in a single boot Windows 7 64 bits without virtual machines. The post was splitted by the moderator, I recommend read these other posts. https://support.industry.siemens.com/tf/ww/en/thread/posts/122558/?page=0&pageSize=10 https://support.industry.siemens.com/tf/ww/en/thread/posts/134722/?page=0&pageSize=10 I'm trying now another solution I post the results later. Best regards. |
Last edited by: miguel_lopez at: 9/28/2015 11:12:02 AM |
|
9/30/2015 1:39 PM | |
Joined: 9/29/2011 Last visit: 6/6/2024 Posts: 23 Rating:
|
Hi everybody. Eventually, I've found a way to fix the problem.
Next I tried to copy the fila with the serial parameters with another name and select in the PG/PC interface and the Microwin starts to comunicate without problem. In order to change the com port, you need to change de xml file, so I create four xml files with COM1, COM2, COM3 and COM4 wich are the most common configuration and create a script to copy this files in the right folder and change the attributes to read only, so the program can not change the settings because, Microwin try to overwrite with the USB driver. I attach the patch in a zip file. The script file instruccionts are in spanish but you only have to press one key twice. You can edit the script if you want. I hope it helps to everyone with the same problem. AttachmentParche Microwin.zip (775 Downloads) |
Last edited by: miguel_lopez at: 9/30/2015 1:42:53 PM |
|
This contribution was helpful to
1 thankful Users |
9/30/2015 1:40 PM | |
Joined: 9/29/2011 Last visit: 6/6/2024 Posts: 23 Rating:
|
I attach screen captures to clarify the post |
9/30/2015 1:41 PM | |
Joined: 9/29/2011 Last visit: 6/6/2024 Posts: 23 Rating:
|
I attach screen captures to clarify the post. |
9/30/2015 1:43 PM | |
Joined: 9/29/2011 Last visit: 6/6/2024 Posts: 23 Rating:
|
I attach screen captures to clarify the post. |
This contribution was helpful to
1 thankful Users |
7/16/2016 6:41 PM | |
Joined: 7/2/2016 Last visit: 7/23/2024 Posts: 1 Rating:
|
I met the same problem with you.I also solved the problem of miss COM port with your method, very good, thank you ! |
Follow us on