1/17/2013 5:11 PM | |
Joined: 11/8/2011 Last visit: 2/22/2024 Posts: 9 Rating: (0) |
Howcan Iopen a existing Microwin file (*.mwp)in the Simatic Manager? |
1/17/2013 5:26 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello Dio; To open a Microwin file, you cannot use Simatic Manager. You need S7-Microwin. The present version is 4.0, SP9. See the Product support page for Microwin: 6ES7810-2CC03-0YX0 What exactly do you need the Microwin file for? If it is to modify a project on the S7-200s, you will need to find out what version was used to program it ( I think projects in version 3.2 cannot be opened by version 4.0, so it wuld be a good information to locate) and you will need a licensed software. If it is only to look at the contents (for analysis or migration to another PLC, for example) then post it here, someone on the forum with the right version of Microwin could make a pdf file for you. Hope this helps, Daniel Chartier |
1/17/2013 6:26 PM | |
Joined: 11/8/2011 Last visit: 2/22/2024 Posts: 9 Rating: (0) |
Thank you very much for this sollution. |
This contribution was helpful to1 thankful Users |
1/18/2013 10:55 AM | |
Posts: 79 Rating: (7) |
NO, You cant, you can just start to make project from that place. |
11/7/2017 8:15 AM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7961 Rating: (162) |
New question published by ron4545 is split to a separate thread with the subject How can get an old MicoWin program converted?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on