8/14/2013 9:57 AM | |
Joined: 6/11/2013 Last visit: 10/7/2022 Posts: 11 Rating:
|
Hello legacy support is it possible to migrate attached s5 plc program. now I'm triying to convert one bye one. but ı have some doubts. during this this time compare s5 and s7 instruction took long time. thanks AttachmentC:\Users\user02\Desktop\S5plcprogram.zip (174 Downloads) |
Last edited by: CS Moderator at: 8/15/2013 3:09 PMnew subject after splitting from /tf/WW/en/Posts/42602#top |
|
8/14/2013 10:44 AM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, Your file is missing a XRF file, this is needed to put the new blocks in the right order. to convert sucesfully you need to prepare the S5 program first. I suggest you read the From S5 to S7 Converter Manual Regards, Marcjan |
Last edited by: Marcjan at: 8/14/2013 10:50 AMProblem solved? |
|
8/15/2013 2:15 PM | |
Joined: 7/15/2008 Last visit: 4/21/2023 Posts: 382 Rating:
|
Hello margow It is possible to migrate to S7, and you should as Marcjian suggested read the manual. I generated the missing S5 XFR file and used the converter to generate the S7 Source Code. S5 Blocks that can not be convrted have benn removed. Please use the S7 Code to check your work. Please note : S5 OB No.= S7 OB No. S5 FB No. = S7 FC No. S5 PB No. = S7 FC No+ 1000 I left an emty FC250 and FC251 in the Program. Please use the corosponding S7 Block from the S7 Libraries for the analog Card you are using. Regards / m.f.g AttachmentC:\Documents and Settings\Administrator\My Documents\S5_to_s7.zip (178 Downloads) |
This contribution was helpful to
1 thankful Users |
6/13/2014 10:21 AM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 177 Rating:
|
Question split intomigrate from S5 to S7 is it possible?. With best regards, Narrator1
|
Follow us on