2/13/2014 12:42 PM | |
Posts: 2 Rating:
|
Hai, Can i convert a program which i had done in s71200 to s7400? |
2/13/2014 1:08 PM | |
Joined: 2/8/2009 Last visit: 8/6/2022 Posts: 56 Rating:
|
not possible to convert s71200 objects in s7 400 |
2/13/2014 2:12 PM | |
Posts: 510 Rating:
|
Here is a link to another forum topic. At the end of the thread, there is a link to download the conversion software. The converter works with V11. You will have to see if it works with V12. /tf/WW/en/Posts/72826 Good luck, billwest |
2/14/2014 5:18 AM | |
Joined: 2/8/2009 Last visit: 8/6/2022 Posts: 56 Rating:
|
Migration tool for TIA v12 is not working for s7200 migration. I cant select .mwp files. Is there any another trick |
2/14/2014 8:32 AM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, You can't just use Migrate, you need to install the Converter Tool The problem is that it is made for TIA V11, so it might not work with V12( as mentioned earlier) Then there is no other option then install V11 and Microwin on a PC, convert the program to V11 and then migrate to V12. Since the converter has it's limits, protected blocks(i.e blocks created with wizard), SMB, etc are not converted, i believe you better spend your time in converting the program by hand or even better write new program that suits the 1200 system. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
Follow us on