9/5/2008 4:23 PM | |
Posts: 133 Rating:
|
Hi Migration errors Subject : Debugging Compiler message : The tag is associated with a connecion that is not available. Current HMI devices on the network: MP370 Touch panel programmed in Protool V6.0 + SP3 Objective: Add WinCC Flexible 2007 + HF4RT station to an existing Profibus Network. I have done the following: 1. Migrated the Protool Project in WinCC Flex 2007 2. I have changed the devie type to WinCC Flexible 2007 RT 3. I have also matched the connection name to the tags connection name. 4. I have added a CP5611 A2 card in the WinCC Flexible Hardware configuration. 5. Netpro compiles with no errors 6. In WinCC Flexible I get 7 Errors saying "The tag is associated with a connecion that is not available." I was wondering ifsomeone could have a look at my program and see where my compilling errors are coming from? The project file is 8MB and I would not beable to upload it onto this website. There is an FTP website : http://www.sendthisfile.com/verify.jsp?lid=JNZy6TUZoJpHU3it4O1AQk0K we could share this file through this website. Cheers |
9/5/2008 4:41 PM | |
Joined: 11/30/2006 Last visit: 3/16/2021 Posts: 118 Rating:
|
Can you please upload the JPG or BMP of Flex Complier . |
Follow us on