4/30/2018 7:30 PM | |
Joined: 3/28/2015 Last visit: 2/15/2025 Posts: 722 Rating:
|
Hello, 1-You need the Configuration program of the panel then you can change the panel type. 2-Uploading the Configuration program only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable back transfer". 3-Backup/Restore with ProSave It is not possible to load and edit a backup file in ProTool or WinCC flexible.The file can only be reloaded to the original or another panel via a restore with ProSave. |
Eng.Mohamed Ibrahim |
|
Follow us on