5/16/2023 6:13 PM | |
Joined: 1/21/2013 Last visit: 4/25/2025 Posts: 3775 Rating:
|
Hi Zed1, Due to the lack of cyclic triggers for scheduled tasks on a Basic Panel, the "GetPLCMode" system function may not be an option. This would only allow the RUN/STOP LED to be mimicked. However, you can use the "LED" instruction within the PLC to provide the state of the LEDs. Note that this would only be possible in RUN mode. Kind regards |
This contribution was helpful to
1 thankful Users |
5/17/2023 12:15 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello Zed1 check this FAQ: https://support.industry.siemens.com/cs/de/en/view/109481628 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on