7/5/2013 1:39 PM | |
Joined: 10/26/2011 Last visit: 12/13/2024 Posts: 762 Rating: (192)
|
If you have engineered the OCX control “PCS 7 redundancy state control” in the process picture as described in the FAQ http://support.automation.siemens.com/WW/view/en/24534102, then diverse graphic objects are not shown completely in the process picture.The missing objects will be shown, if you track an additional window (e.g. a TagLogging OCX) over the screen. Alternative Solution 1. Set the attribute “Display“ of the redundancy state control to FALSE (see attachment) 2. Open the object properties of the picture (diagnostic.PDL) and engineer in open picture a direct connection, which set the appropriate attribute (Open Picture) to TRUE. (see attachment) |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
Follow us on