Industry Online Support
Technical Forum
10/17/2012 10:29 AM | |
Joined: 12/2/2008 Last visit: 3/21/2024 Posts: 12 Rating: (0) |
Dear Team, System configuration : PCS7 V7.0,CFC V7.0,F System V6.0,Safety Matrix V6.1 I have purchased the above mentioned FDO module for one of my existing project for expansion purpose. In the same project we are using the FDO MLFB: 6ES7326-1BF01-0AB0 modules and new module MLFB: 6ES7326-1BF10-0AB0. I have updated the F Configuration tool V5.5SP6 or higher for configuration. The tool can be downloaded directly from entry ID 15208817. Now i am able to communicate the module and online shows that the module available and ok. We tried to Force the DO from CFC Chart but the output is not getting on. Also tried with WinCC and given the comment to open the valve,it shows QBAD. Now what should i do for making to work this module. Best Regards R Ranganathan |