4/10/2016 9:10 AM | |
Posts: 8946 Rating: (999) |
Strange question... You may use this tool, free of charge. Working with MC also: |
This contribution was helpful to3 thankful Users |
4/10/2016 5:36 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
1. You are not able to read / delete it in the SIMATIC MMC reader/writer of a Siemens PG or a Siemens External EPROMMER. 2. The MMC does not work even after you reset it with the following procedure : How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? Hope this helps Cheers |
There is no such thing as the last bug in a program |
|
This contribution was helpful to3 thankful Users |
4/11/2016 8:40 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello ANKURGAMIT, Try to make Operating System Update for your CPU. I hope it will solve your problem. If not, then send it to your Supplier or local Siemens Office for repairing or replacement if you are in warrenty period.. Where can you find the latest updates of the operating systems for the CPUs S7-31x |
Ayman Elotaify |
|
4/11/2016 9:38 AM | |
Posts: 8946 Rating: (999) |
If CPU is 1200 or 1500 you may check the physical card with or Windows tools without problem. But do not try to format them. See here: |
This contribution was helpful to2 thankful Users |
Follow us on