Industry Online Support
Technical Forum
2/23/2008 12:10 PM | |
Joined: 4/6/2006 Last visit: 1/21/2019 Posts: 604 Rating:
|
Hello, When you want to use the full functionality of the 315-2 PN/DP FW: 2.6 you need at least Step 7 v5.4 SP2. If you have an older version you won't be able to use/download the HSP's for this FW version. Normally a 2 Mb MMC will be sufficient for this CPU but it depends on the program you create and the items you want to store on the MMC. Also have a look at the following URL, because there is an update available for the CPU ou use. http://support.automation.siemens.com/WW/view/en/23876897 |
Best regards, |
|
Follow us on