4/29/2019 1:45 PM | |
Posts: 3093 Rating:
|
Hello, I recommend to use the newest version of the library for your project. It is the library 6AV6676-6MB30-4AX0. This library supports hot standby. These technical data apply: Regards, |
This contribution was helpful to
1 thankful Users |
4/29/2019 2:47 PM | |
Posts: 4 Rating:
|
CP IS A SERVER I HAVE TO HIGHLIGHT THAT THE MODBUS IS WORKING BUT FOR THE CPU WHICH IS THE MASTER AND FOR THE STANDBY CPU NO TX/RX IS FAST BLINKING. AND WHEN I SWITCH OVER THE CPUs THE CP OF THE OTHER RACK STARTS THE TRANSMISSION AND RX/TX BLINKS TO SHOW COMMS ARE OK BUT AT THE SAME TIME THE OTHER CP SHOWS RUNNING IN DIAGNOSES BUT ITS NOT UPDATING MODBUS DATA. I USE MODSCAN TO CHECK THE DATSA ON BOTH CPs. THE CP WITH THE MASTER CPU IT SHOWS THE DATA BUT THEONE ON STANDBY CPU ITS NOT FIND ATTACHED THE DIAGNOSES AttachmentDiagnose CP1 29042019.txt (129 Downloads) |
Last edited by: Filimone F at: 04/29/2019 14:55:59 |
|
4/29/2019 4:29 PM | |
Posts: 4 Rating:
|
MANY THANKS. I WILL WORK ON THE CLIENT SIDE SO SORT THE PROBLEM |
Follow us on