10/6/2010 5:04 PM | |
Posts: 12 Rating:
|
I want to made aModbus communication over Ethernet with my S7-1214. I tried to use the PAClibrary to configure that communication. To prove that it works, i used the "QuickMod Modbus Scanner" but I can´t to communicate with then. I wanna know if it´s possible that communication with this library or how i need to configure that module to get the right communication. Thank you. Splitted from Modbus over ethernet TCP communication possibilities on S7-1200 ?. |
Last edited by: O_Moderator at: 10/7/2010 12:24 PMnew subject after splitting |
|
10/13/2010 5:44 PM | |
Posts: 3093 Rating:
|
Hello Tresancos, as far as I can see in the QuickMod flyer, it is a tool to monitor the data traffic not to simulate a Modbus Server. Regards, Kaulquappe |
Follow us on