7/1/2015 7:33 AM | |
Joined: 2/24/2011 Last visit: 2/25/2025 Posts: 86 Rating:
|
Here is my code. Currently I'm doing COM_RST of FB640 and FB641 manually, as it is not fully functional piece of code. When I call a FB641 with DATA_ADDR = 40001, I receive an error code 8189. When I call a FB641 with DATA_ADDR = 1, I receive an error code 8382. Eurotherm controllers allows to use function 16 for block write operations, and functions 3 and 4 for reads. In the doccumentation of Eurotherm controller Modbus addresses in decimal are from 1 to 1291 and from 12290 to 13090. Where the function numbers are used in the FB641 and do I need to use 40001+Eurotherm Modbus addresses or just Eurotherm Modbus addresses in FB641 DATA_ADDR input? AttachmentPrintout1.pdf (394 Downloads) |
Follow us on