1/20/2013 5:51 AM | |
Posts: 24 Rating:
|
Hello, I am using two Modbus RTUs CP 341-RS 422/485 in my system consisting of S7-400 cpu's (hot redundancy). In my configuration I have configured my 1st cp341 as a master and the second one as a slave.Master will fetch data from the slave. Have inserted the Dongle and have also parameterized both the master and the slave.But while loading the respective drivers in the CP 341,I get error msgs 2248:2004 (showing unable to read module status) and error 2248:2016 (showing driver update canceled because of error).Getting this error while loading drivers in master and slave.Please help. Have attached the error messages. Attachmentmodbus_error.zip (462 Downloads) |
1/21/2013 1:31 PM | |
Posts: 3093 Rating:
|
Hello Jigarhg, with the latest version of CP341 it is not longer necessary to transfer the Modbus driver to CP341. Just have a look at this FAQ. You shouldparameterize the Modbus driver for the CP and transfer the parameterization to the CPU. Regards, Kaulquappe |
This contribution was helpful to
1 thankful Users |
7/13/2015 2:16 PM | |
Posts: 3093 Rating:
|
I think you need the latest version of PTP-Param as well.
Regards, |
9/8/2015 12:33 PM | |
Posts: 1 Rating:
|
hi sorena87 i have your same problem .... could u solve your problem at least? |
10/20/2015 2:15 PM | |
Posts: 247 Rating:
|
Dear Experts, I am also facing the same issue.I am not able to download the drivers in CP module but I have downloaded it early without any issues. |
Follow us on