6/8/2009 3:28 PM | |
Joined: 2/6/2009 Last visit: 1/7/2025 Posts: 939 Rating: (118) |
Hi, There is no big difference between CP341 & 1SI. You can use the same logic of the CP 341 for the 1SI. The only thing is that you have to change the Send/Rcv blocks from FB7/FB8 to FB2/FB3. Please find the attachment for the library blocks of the 1SI. If you want any sample program of CP 341, just send one mail to me and I will send the Sample program. Attachment1Si Modbus Blocks1_V122.zip (395 Downloads) |
_______________________________________________________________ |
|
9/2/2015 3:55 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by mushtaq is split to a separate thread with the subject Sample program for ET151-1 Standard with modbus master communication. Best regards |
Follow us on