3/16/2017 3:10 PM | |
Joined: 4/28/2015 Last visit: 3/26/2025 Posts: 10837 Rating:
|
Hello, you can look to this link: Also as standard CP341 MB RTU Master manual can be helpful, there you can see what you need set to correctly receive data from Slave. Attachments7300_modbus_master_operating_instructions_en-US_en-US.pdf (744 Downloads) |
Last edited by: Duris_I at: 3/16/2017 3:10:47 PMWith best regards... |
|
3/16/2017 3:42 PM | |
Joined: 9/27/2006 Last visit: 3/26/2025 Posts: 12344 Rating:
|
Hello R_Romero; I agree with Panov69, you might have overlooked the required step to load the Modbus driver in the CP 341. For this, you need the Setup_PTP package, that you can download from this FAQ: Download CD 'CP340, CP341, CP440, CP441' Also check section 4.7 "Assigning Parameters to the Loadable Driver" of the Modbus master driver manual that was suggested by Duris_I in his earlier post Hope this helps, Daniel Chartier |
3/16/2017 6:00 PM | |
Joined: 11/17/2010 Last visit: 9/12/2024 Posts: 216 Rating:
|
Sorry, my mistake I found a FAQ talking about that : Loadable driver CP341. |
Follow us on