10/13/2010 8:43 AM | |
Posts: 86 Rating:
|
Hi, which hardware do you want to use? Monty |
10/13/2010 8:58 AM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating:
|
Hello, under the following link you can find the manual forSIMATIC S7MODBUS Master: http://support.automation.siemens.com/WW/view/en/1220184 under the following link you can find the manual forSIMATIC S7MODBUS Slave: http://support.automation.siemens.com/WW/view/en/1218007 You can use the modbus driver with the serial CPs CP341 and CP441-2. In the manuals you can find information about commissioning the driver, useable moduls (chapter 2.2) and application examples. Best regards Little Holmes |
This contribution was helpful to
1 thankful Users |
Follow us on