10/9/2012 8:05 PM | |
Joined: 9/27/2006 Last visit: 3/17/2025 Posts: 12344 Rating:
|
Hello Hit_Formula; Error code Hex 0837 on the 1SI module refers to a "Message frame sequence error", see the attached screencapture, from the SIMATIC ET 200S Serial interface modulesmanual. Try to increase the slave timeout parameter as proposed in the manual. See section 3.5.3 of the mentionned manual, Configuring and setting parameters for the Modbus master, page 144, Response time. Hope this helps, Daniel Chartier |
10/10/2012 3:35 AM | |
Joined: 2/20/2010 Last visit: 2/19/2025 Posts: 104 Rating:
|
Hi dchartier, I had increase timeout and make with 3000ms after that I got error message 08 30h. |
10/10/2012 11:33 AM | |
Posts: 3093 Rating:
|
Hello Hit_Formula, do you use RS485 interface? If yes, I guess you connected R(A) and R(B) vice versa. Regards, Kaulquappe |
2/20/2014 11:41 AM | |
Posts: 340 Rating:
|
new question is splittet to i'm having some problems communicating with a weight indicator |
12/16/2014 8:32 AM | |
Joined: 3/7/2007 Last visit: 2/19/2025 Posts: 3 Rating:
|
Hello Hit_Formula I've the same problem witha Kamstrup Multical energy meter. Do you find a solution? Best Regards
|
Follow us on