10/3/2015 2:43 PM | |
Posts: 86 Rating:
|
Hi to all,
I'm reading the density value as shown in Flow.jpg into %MW100(2 registers) this far everything OK(the value is Float and not swapped), and other modbus master will read it from my list in PLC but here starts a problem. if i leave the density value in %MD100(%MW100 - LSW and %MW101 - MSW) the values are not readable and not representing any thing. So i swapping the %MW100 and %MW101 as shown in PLC.jpg, in this case the values that i read are more relevant but still having a problem as shown the difference between modbus.jpg and modbus2.jpg. Im using CM1241 485 module.
any ideas would be great.
Attachmentmodbus.zip (375 Downloads) |
Last edited by: Estring at: 10/3/2015 2:47:03 PM |
|
Follow us on