4/25/2019 9:23 AM | |
Posts: 6 Rating:
|
hello people I have a very interesting problem with my modbus communication between these two PLCs. the 1215C is MASTER and Fatek is slave. The function in 1215C reads 10 Words from Fatek. there is a pointer to M530.0 to put the data into when it reads it. when I change the word in my slave two words on the master change and I dont know why. i dont understand the problem. why is there a change in a 32bit length area of memory? Attachment2019-04-25_11-30-52 (convert-video-online.com).avi (171 Downloads) |
5/1/2019 10:19 AM | |
Posts: 6 Rating:
|
the project is running fine. but I am just wondering why I have this problem? is there a problem with my function or the protocol from Fatek side has a problem. |
5/19/2019 9:54 AM | |
Posts: 3093 Rating:
|
See attached screen shot. Regards, |
This contribution was helpful to
1 thankful Users |
5/19/2019 10:57 AM | |
Posts: 6 Rating:
|
so the 16th bit of MW0 is MB0.7? How is this Logical? Im Not saying its not I just cant see it! |
Last edited by: pcm63 at: 05/19/2019 11:00:26 |
|
Follow us on