11/16/2016 10:08 PM | |
Posts: 3 Rating:
|
Hi everyone, I'm trying to stablish a modbus RTU comunication Master-Slave, the hardware as follow: CPU1214 AC/DC/Rly CM 1241 (RS422/485) 1CH32-0XB0 firmware choosen in hardware configuration is V2.0 Ekor RPG relay Ormazabal The problem that I have is, altough I see that the comunication chanel is ok when configured I don't recieve any kind of data. The TX Led indicator on CM is always flashing orange and when i call de MB_MASTER that also is selected a V2.0 version. Busy indicator of the FB always is activated because I'm using system flag for 5Hz to make a Request to the Slave, and the Error bit and Status byte form the function block always are 0000. Best Regards, AttachmentMB_MASTER.zip (59 Downloads) |
Follow us on