11/1/2012 1:20 PM | |||||
Joined: 9/27/2006 Last visit: 3/18/2025 Posts: 12344 Rating:
|
Hello m. shoaib khatana; The CP 341 you have selected has a RS-422/RS-485 interface, so you cna connect to up to 31 slaves having the same interface (either all on RS-422, or all on RS-485; make sure they are conforming to the electrical interface standard). The license you have selected is a Copy license, I suggest you purchase the complete license, shown below. A full license comes with the parametrization software, documentation and sample projects. A copy license only has the dongle and the license key, so it is good for installation on multiple CPs once the program is ready (one for each CP). You can look up details and manuals for both products on these links:
Hope this helps, Daniel Chartier |
||||
Last edited by: dchartier at: 11/1/2012 1:43 PM |
|||||
11/1/2012 5:36 PM | |
Joined: 10/31/2011 Last visit: 11/26/2024 Posts: 400 Rating:
|
Dear sir, Can i use cp340 with rs485 interface for rtu communication by writing own driver?
|
11/1/2012 6:03 PM | |
Joined: 9/27/2006 Last visit: 3/18/2025 Posts: 12344 Rating:
|
Hello m. shoaib khatana; There is nothing stopping you from doing so. However I would caution you that it is not so easily done. Have a look at smiffy's reply to this threa, especially on the time it took to develop, test and implement the driver(and he will not send his code to another forum member, it has already been requested): CP 340 communication with RS-485 modbus Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on