12/9/2013 5:05 PM | |
Posts: 3 Rating:
|
Hello, I have CPU 1215+CM1241+CB1241 configuration with TIA V11 SP5. I tried to communicate with some energy measurement devices but could not do it from both devices. I communicated correctly with SW on PC and some RS232 to RS485 convertor. Problem: I tried that CM is master then CB is master (both situation only with one of them), in both situation TX led is blinking but there is no response. Then I connected sniffer to modbus I noticed that in some situation 2 byte are transmitted in some 3, not 8 as defined in protocol. Could see that one of them is address, because it changed in same waywhen I change address in SW. TNX and regards Damir AttachmentMODBUS_MASTER_problem.zip (139 Downloads) |
Follow us on