8/4/2015 1:24 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Think about the following: CPU315 PN ==> X104-2 ==> FO ==> X104-2 ==> ET200M for PN The CPU act as PNIO controller. The X104-2 is a switch with two FO ports. The CP341 (with Modbus dongle) acts as Modbus Master and you start here a local RS485 Modbus Bus. As alternative to the ET200M + CP341, you could think about a S7-1200 as i-device of the CP315PN. |
Last edited by: jklm at: 8/4/2015 1:26:31 PMBest regards |
|
This contribution was helpful to
2 thankful Users |
8/5/2015 2:43 PM | |
Posts: 9 Rating:
|
Sorry sir, wrong attachment. I'm just confused with the arrows below. Did you use a separate et200m with a cp341 for modbus rs485 interface? |
Follow us on