9/8/2016 9:51 AM | |
Posts: 2 Rating:
|
Hi everybody! I'm trying to communicate by RS-485 modbus a TLB485 (slave) with s7 1200 (master) using the CB1241 integrated at the CPU s7 1200 1215C DC/DC/RLY. However, when I use the COMM_LOAD module, I get "ERROR 16#8180: Invalid port ID". I'm using as port in the COMM_LOAD "PLC(1)" because its ID is 269 (the same as the ID of the CB1241) so I don't understand what is the problem. In the pics you can see all that I mean. I have read the sample project for modbus and other topics related without get a solution. Please, help me. Thank you very much! Attachmentpics.zip (619 Downloads) |
This contribution was helpful to
1 thankful Users |
9/8/2016 12:42 PM | |
Posts: 2 Rating:
|
Thank you very much. There was a beginner problem. I have changed that and now work! |
This contribution was helpful to
1 thankful Users |
9/8/2016 8:44 PM | |
Posts: 64 Rating:
|
Waav mopS04 perfect eyesight |
This contribution was helpful to
1 thankful Users |
Follow us on