3/31/2023 5:20 PM | |
Joined: 9/14/2020 Last visit: 1/8/2024 Posts: 8 Rating:
|
Hello! I need help with the following: I need to read data from 5 slave devices. The problem is that, for example, when data is being read from slave 1 to a buffer, it is then converted to another data type and stored on a data block. But when data is being read from another slave, it will overwrite the data stored on that same datablock. I tried to create a test condition to move the data on the buffer to the correspondent address on the DB only if slave 1 is being selected for reading, and the MB_Master_DB Done output is set to 1 but it didnt work. I have the images of the code are attached on a zip file. Attachmentprints para forum tia portal.zip (395 Downloads) |
Follow us on