11/25/2017 12:52 AM | |
Joined: 6/13/2011 Last visit: 2/19/2025 Posts: 6 Rating:
|
Hello everyone I need to communicate two PLCs, the first one is an S71200 PLC (slave), the other is a Modicon TM221 PLC (Master), I have made the configuration in both PLCs, and I have tested them separately using the ModBusPool software, and it works normally, however, in the communication tests between both PLCs, the link is established, but there is no data exchange, please if someone can give me a clue as to what may be happening, I enclose screenshot of configuration. Thanks AttachmentModbusTcp.zip (234 Downloads) |
Follow us on